This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563201: Short test. Alternate part

Part Number: TPS563201
Other Parts Discussed in Thread: TPS561201, TPS562201

Hi team,

Customer has seen TPS563201 went broken when they short the output. They found OCP work well but the repeated OCP due to hiccup protection cause damage. Is customer thought correct?

If so, they are looking for other parts with lower OCP OR latch off OCP.

Could you please let me know the buck converter with below spec?

Vin: 16.5V

Vout: 3.3V or 5V

Iout_max: 0.4A

Latch-off OCP OR 1~2A OCP thrshold

Regards,

Hayashi