This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS254900A-Q1: TPS254900-Q1 about resistor and cap setting question

Part Number: TPS254900A-Q1
Other Parts Discussed in Thread: TPS254900-Q1

Hi, Support Team

There are some questions for TPS254900-Q1 as below:

Since there is no down device for connect to TPS254900-Q1 5V output in out design.

Q1: Want to know how to deal with pin:12 BIAS? 5.1Kohm pull-up resistor & 2.2uF capacitor still necessary?

Q2: Want to know how to deal with pin:1 IMON/pin:19 ILIM_LO/pin:20 ILIM_HI?

Q3: Is it required for DP/DM signal pull-down with 10K or 15K ohm resistor?

Q4: Want to know how to deal with pin:6 CS if not used?

schematic:

if any suggestion, Please advise me.

Thanks,

Best regards,

Lawrence

  • Hi Lawrence,

    Good questions.

    Below are my comments:

    1: Yes, this pin is used for IEC protection, so please keep them.

    2: The MON is a current source, so please don't float it, please add a 2.55Kohm in this pin. For the pin:19 ILIM_LO/pin:20 ILIM_HI, these both pins are used to set the current limit, so you can short to GND to set maximum current limit.

    3: It depends on whether the host side have this resistors, if not, please add them.

    4:Just floating it.

    Best Regards,

    Kuno