This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119EVAL: Operation different from User Guide

Part Number: LM25119EVAL
Other Parts Discussed in Thread: LM25119

Hi!

I just ordered a LM25119 Dual Buck Regulator Evaluation board and began testing it today. I was reviewing the user guide before starting my testing just to make sure I had the correct connections and everything. When I began testing I noticed my values on the output were significantly different than what the user guide stated. 

User Guide Values: 

Channel 1 --> 3.3V @ 8A 

Channel 2 --> 1.8V @ 8A 

Measured Values:

Channel 1 --> 10V @ 6A 

Channel 2 --> 5V @ 8A 

Is there a different User Guide that I am supposed to be looking at? Or was there a change to the board that was not reflected in the Users Guide? I just want to make sure I am not going to ruin the board as I begin to test the interleaved operation. Thanks!