Other Parts Discussed in Thread: LM25119
Hi!
I just ordered a LM25119 Dual Buck Regulator Evaluation board and began testing it today. I was reviewing the user guide before starting my testing just to make sure I had the correct connections and everything. When I began testing I noticed my values on the output were significantly different than what the user guide stated.
User Guide Values:
Channel 1 --> 3.3V @ 8A
Channel 2 --> 1.8V @ 8A
Measured Values:
Channel 1 --> 10V @ 6A
Channel 2 --> 5V @ 8A
Is there a different User Guide that I am supposed to be looking at? Or was there a change to the board that was not reflected in the Users Guide? I just want to make sure I am not going to ruin the board as I begin to test the interleaved operation. Thanks!