Hi,
I' am using the TPS65185 to supply the Eink display (whose specification is in accordance with the PMIC specification). We use an Epson S1D13524 connected by I2C to your PMIC to drive the display.
When we are issuing the "black/white" command (to clean the display), sometimes (randomly, but rarely) it fails and the pwr_good signal goes to 0.
In this case, register value for INT1 is 0x00 and INT2 is 0xC0 or 0xC8. We are looking for what is wrong in our design and we need some clues. We are not sure if the issue is from the input power supply or the PMIC (3V8 in our case) or if it is from the elink display which need important inrush current (so the pmic can not supply enough).
I have performed measures and as you can see on the picture below, we found one of the reason why the pwr_good signal goes to 0. The blue trace is VDDH (+26.4V) and the red trace is the pwr_good signal. It seems that the eLink display needs a rush current for a short time (So VDDH goes below 90% of its nominal output voltage and the pwr_good goes to 0)...
- What is the delay between the fault detection and the pwr_good assertion ? In our case it seems to be about 2ms (see the picture below).
- In the datasheet there is a "power good timeout" parameter set to 50ms. Does it mean that if the undervoltage lasts less than 50ms, the pwr_good signal stays at 1 ?
- Last question, if for example there is an undervoltage on VDDH_IN (pin 37), is pwr_good signal asserted to 0 ?
Thank you for your help
Best regards, Pascal