Hello,
At TPS25831-Q1, which runs first when a device is connected to DFP via a cable, detecting CC for Type-C or the auto-detect state machine that supports all DCP charging schemes?
Best regards,
K.Hirano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
At TPS25831-Q1, which runs first when a device is connected to DFP via a cable, detecting CC for Type-C or the auto-detect state machine that supports all DCP charging schemes?
Best regards,
K.Hirano
Hi K.Hirano,
It should be the CC detected first, and then start the auto-detect state machine, because the BC1.2 need the VBUS first, so we need to finish the CC handshake, and power on the VBUS, then will start the DCP machine.
Best Regards,
Kuno