This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX660: Output failure mode

Part Number: MAX660

Hi Team,

Can you please help with this inquiry of our customer?

My associate is claiming this part has a fault condition whereby the inverted output can go positive during start up mode 

I.E. as a +3 to -3V converter that during start up the output goes positive and tracks the +3V input. He suggests we add a protection diode to Vout to block this .. I am having difficulty understand how this could be possible, any thoughts?

"add Schottky (ZLLS410TA) diode from -3V to GND to prevent -3V bus form going positive in startup and fault conditions."

Regards,

Danilo