Other Parts Discussed in Thread: BQ76940
Dear Sir or Madam,
I have the following problem.
We have an end customer who assembles batteries with our printed circuit boards.
This is a 10S2P battery.
On the PCB there is a BQ76930 and the communication BQ 78350.
In our firmware PF_EN, LIFETIME_EN and BBR_EN are already set before the battery is assembled.
Is it possible that any errors are set during the assembly of the battery and thus the cells are possibly discharged via the balancing fets?
After about two weeks after the assembly, the cells 6-10 sometimes show a very low voltage.
Image:
Our customer has a failure of about 30% of the assembled batteries.
An analysis could not find any defect on the PCB.
Attached are a few screenshots of the circuit.
Thanks in advance.