This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB-C-PD-DUO-EVM: Are there any softiscastet templates that work on TIDA-050014/USB-C-PD-DUO-EVM

Part Number: USB-C-PD-DUO-EVM

We bought the USB_C_PD_DUO_EVM for testing a development object we produce. Well I don't undestand how to configure this thing and the information needed for that is not seemable bundled so I failed after 3 hours of researching to get some succes. 

My goals: 

I need a power sink, where I can switch between 5V,9,15 and 20V by pushing a button.

What I tried: 

I loaded the TEMPLATE for the TIDA-050014 SINK-Board and tried fashing it into the device, but it doesn't work? By pressing any buttons it just doesn't do anything. I already did what the manual said(design guide of EVM) and put the little junction at snk. And then I tried updating the standard template into the board. It doesn't work. I only need the sink board for my testings... Well I really don't get how to configure the registers. There are too many informations and I think u need a whole semester to get fully into this. 

My question is:

Does someone have a template that actually works and does what I am aiming for?

Thank you.