This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z655-R1: BQEVSW bqCHEM Tab issue

Part Number: BQ20Z655-R1
Other Parts Discussed in Thread: BQEVSW, EV2400

Greetings,

We have an issue with bqsw software bqCHEM tab. We have selected the correct battery chemistry for our cells using the Chemistry Selection table. After closing the program and re-opening it, when we navigate to the bqCHEM tab, we get an error message that says Cell:Obsolete (Do not use) Failed to add to chemistry selection table. On the message title it says: Syntax Error in Chem.ini. 

Are these errors a program bug, or is there something wrong with our data flash etc?
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/Screenshot-2023_2D00_03_2D00_08-154256.jpg