This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62745: I need a buck converter with similar spec of above mentioned part number, but with a different out put voltage and temperature

Part Number: TPS62745

Specifications: 

Input Voltage: 1.8,2,3.3V- 30V

Temperature range: –55°C to 85°C

Output current: above 6mA 

Switching Frequency: Should be greater than 100KHZ

Ripple frequency: In the range of 100KHZ

Buck converter with intrinsic safety feature is required(Lower value inductor(Max 10uH) and Lower value capacitor(20uF-sum of CIN and COUT)