Hello E2E Experts,
Good day.
I am using the LM5158QRTERQ1 in the SEPIC configuration outputting 25V. I've been trying to find a good capacitor to use for my output capacitor that also doesn't take up too much space, but it seems like most of the available ceramic capacitors have a large capacitance change rate at 25V. It mentions using a ceramic capacitor in the datasheet, but I was wondering if I can use a tantalum capacitor instead. According to the QuickStart excel sheet provided by the datasheet, I need 40uF of output capacitance to meet my desired ripple voltage, which generally either comes in a very large package or with a low voltage rating for ceramic capacitors.
The datasheet mentions using ceramic capacitors but doesn't explicitly say to not use tantalum. I am wondering if it would be ok to use a tantalum capacitor instead.
Regards,
CSC