Hi team,
I have two questions about single-end use.
1. The data sheet requires to connect a local bypass capacitor, but where does this capacitor connect?
2. VSNS- and AGND are connected in the shortest trace.
Can they connect both to the common GND pattern, or should they be wired separately from the common GND?
– For single-end sensing, connect the higher FB resistor to a high-frequency local bypass capacitor of
0.1-μF or higher, and short VSNS– to AGND with shortest trace.
Best Regards,