Other Parts Discussed in Thread: UCC28950
Hello TI wizards!
I have a requirement for an isolated DC-DC converter with an input of 350VDC to 400VDC and an output of 380VDC at 8A max. Is this something the UCC25630-1 could handle? If so, would you have any suggestions on beginning the design? The spreadsheet doesn't seem to handle this combination of requirements. If sot, could you point me in the right direction? Any help would be much appreciated! Thanks...