Other Parts Discussed in Thread: BQ21061
Hi
I have battery connected to BQ21061 as in the following schematics. When I connect the battery without usb connection. The BQ21061 should be in shipment mode by default and draw nano amp current. However, I get 4.5mA of current and the output VCC is 1.3V. I have the circuit on a custom pcb and it is not possible for me to measure how much current is draw on the rest of the circuit.
When I click the MR button to start it, it goes down to a reasonable level around 300uA. Would you please help me find the possible reason the sleep mode current is so high.
I've measured my circuit resistance at the battery port without battery connection. The resistance is in >200kOhm range.