This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
the TLVM13620 should as per DS comply with CISPR 32 class B emission, is this only for radiated emissions? and for conducted emissions it still needs an LC filter on input?
Because when i load the TLVM13630 design in Webench and try to add the EMI filter and select for CISPR 22 class B it doesn't meet the standard, it is above limits so LC is needed to pass CISPR 32 class B conducted emission ?
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=447CE7719F3AEB18
Best Regards,
d.