Other Parts Discussed in Thread: GPCRB
Dear expert,
My BQ27Z561R1 works fine for both 25C and -10C temperature.
However, when temperature suddenly jump from -1C to -10.3C as below table in yellow, SoC jump from 18% to 16%.
How to avoid this? I already enabled smooth engineer.
Temp | Vbat | Ibat | AIbat | Rm | Soc |
284 | 3634 | -1019 | -877 | 918 | 19 |
287 | 3610 | -1124 | -936 | 916 | 19 |
290 | 3593 | -1275 | -1010 | 915 | 19 |
292 | 3613 | -1072 | -1047 | 913 | 19 |
297 | 3625 | -814 | -1023 | 912 | 19 |
298 | 3650 | -820 | -962 | 911 | 19 |
295 | 3723 | -259 | -823 | 910 | 19 |
85 | 3769 | -33 | -13 | 901 | 19 |
-10 | 3772 | -9 | -13 | 882 | 18 |
-103 | 3761 | -12 | -10 | 764 | 16 |
Below is DFFS file I used.