This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34936EVM: withstand voltage of D4 and D5

Part Number: LM34936EVM

Hi support team,

The withstand voltage of D4 and D5 is 100V, but under the following usage conditions, is it okay if the withstand voltage is low (about 30V)?

Vin: 10~17V
Vout: 12V
Iout: 3~4A

Regards,
Dice-K