This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25011-Q1: UVLO Range for Falling

Part Number: LM25011-Q1

What is the falling range of the UVLO device.

  • Hi Shubham,

    You can refer datasheet as below:

    When Vin > UVLOVIN=5.3V, the regulator begin to output .

    Then when Vin < UVLOVIN-V-threshold hysteresis=5.3V-200mV=5.1V, the regulator stops running.
     So falling range of the UVLO device means the voltage that makes regulator stop running. 

    I

    Thanks 

    Colin