hi teams:
12V IN 5V_ There is an inductive noise during the output process of out 0.3A-0.6A
Inductive saturation current 3.8A.
Help point out how to modify to solve the noise problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi teams:
12V IN 5V_ There is an inductive noise during the output process of out 0.3A-0.6A
Inductive saturation current 3.8A.
Help point out how to modify to solve the noise problem?
Hi Kevin,
We see the switching frequency should be around 400kHz which will not cause acoustic noise. Can you check if there exists low frequency ripple in the circuit? You can have a test of Vin IL SW and Vo to see if they are stable? I also suspect inductance noise come from L100 and you can remove it to check again.
Thanks
hi Colin:
1. We will attempt to adjust the power frequency to 400K;
2. We previously changed L100 to a short circuit at 500K, but the sound still exists, mainly on L101,