In the board which we used the LP8869C-Q1 has the switching noise in the input (VIN) with respect to the Brightness PWM control frequency and duty cycle except the 0%,100% duty cycle.
The Noise is in the range of approximately 400mV to 1V peak-peak based on the different PWM frequency.
To understand this issue, We tested with the TPS61194-Q1EVM ( LP8869C-Q1 assembled on it ) and observed the similar switching there on EVM input also.
Please support on this issue, to mitigate the noise in the input with brightness control PWM change.
Thanks in advance.
Regards,
Surya