Hello E2E Experts,
Good day.
In the datasheet, I will be referencing sections 7.4.1 and Figure 14.
In the datasheet section 7.4.1, it suggests using a resistor of low value (around 100Ω), but I have tried using higher values to create the feedback loop for Vref and it doesn't work. I would like to know the highest values for R1 that will work, in order to reduce the overall current flow on the device.
Specifically, I need to know the highest value that R1 can be.
Seems the resistor values are far too high. This doesn't work. The math is all right, but I realized today that section 7.4.1 wants something lower.
The problem with lower values, as you may see already, is that it can lead to a lot of current drains.
Again, all I need to know is the highest value R1 can be to create the 1.25V ref voltage. The values I have now do not work and I am referencing 7.4.1.
I need 3.3V, 4.1V, and 5V with three separate LM1084s.
Regards,
CSC