Other Parts Discussed in Thread: TPS65982, TPS65981, TPS65987
Hi,
I designed a board using TPS65987, it sources 5V or 12V through PP2 and sinks 5V or 12V through PP1. It can work with TPS65982 or TPS65987, the voltage will switch from 5V to 12V after PD negotiation between them. But it doesn't work with TPS65981, it looks like there's no PD negotiation between 65981 and 65987 or their negotiation is unsucessful. Because our old products are using TPS65981, we have to make them work together. Can you give some advice to this problem?