Part Number: LM5157EVM-SEPIC
Other Parts Discussed in Thread: LM5158
I was trying to use the LM5157EVM-SEPIC board to test the LM5158QRTERQ1 part. I am trying to test with an input range of 17V-60V and output 25V, so I made some modifications to the board, but it failed when I applied 60V.

Here are the parts that I replaced and what I replaced them with
U1 – LM5158QRTERQ1
L1 – SRF1260-220M
D1 – PMEG6030EVPX
C8 – GRM31CC72A475KE11L X2
Input Caps – GRM31CC72A475KE11L X2
C21 – GRM155R62A104KE14D
R6 - ERJ-2RKF4702X
R9 - ERJ-2RKF1961X
Are there any parts that I missed that need to have a higher voltage rating or is there a different problem?
Thanks
Garrett