Other Parts Discussed in Thread: LM5010, LMR38020
Hello,
I'm working with LM5010AMH/NOPB. Side note - the E2E forum did not seem to recognize this as a valid PN, so I had to enter LM5010A.
Per the datasheet section 7.3.2 the UVLO is set to 5.25V.
I have the part configured to regulate to 9.00V.
The part works perfectly fine when Vin exceeds the desired 9Vout.
The issue I'm seeing is if the input Voltage is ramped up from 0V. Once the UVLO of 5.25V is exceeded the part attempts to begin regulating, and we see an output starting at ~1.5V and this walks up slowly tracking Vin until we get into a stable mode where Vin exceeds the desired output.
I'd like to configure this part to output 0V until it is capable of putting out a solid 9.00V. In other words, is there a method to change the UVLO of the part to something like 9.5V? Any other ideas on approaches to keep the output "off" until we have sufficient Vin to be in a stable control mode?
Thanks in advance!!
The schematic is below