we are using a TPS6590378ZWSR PMIC along with the TMP102AIDRLT Temp sensor.
We copied this from the EVM schematic that was based upon using the TPS6590376.
The Temp sensor and the PMIC both use 0x48 address, but in the data sheet for the PMIC it says if there is a bus conflict the PMIC address can be 0x58.
How is this accomplished? Is this something that needed to done by the factory? Is there a strap bit?
Thanks,
Mark Zeid
Principle Hardware System Engineer
Ossia Inc.
2681/2683 151st Pl NE, Redmond, WA 98052
M: +1-425-677-5224