This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659037: TPS659037

Part Number: TPS659037

we are using a TPS6590378ZWSR PMIC along with the TMP102AIDRLT Temp sensor.

We copied this from the EVM schematic that was based upon using the TPS6590376.

The Temp sensor and the PMIC both use 0x48 address, but in the data sheet for the PMIC it says if there is a bus conflict the PMIC address can be 0x58.

How is this accomplished? Is this something that needed to done by the factory? Is there a strap bit? 

Thanks,

Mark Zeid

Principle Hardware System Engineer

Ossia Inc. 

2681/2683 151st Pl NE, Redmond, WA 98052

M: +1-425-677-5224