Other Parts Discussed in Thread: UCC28730
With an input voltage range of 9-16V and serving a load of 32W by multiple secondary windings, if yes is there a reference design available?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
With an input voltage range of 9-16V and serving a load of 32W by multiple secondary windings, if yes is there a reference design available?
Hi Sal Pavan,
The UCC28730 can be used as a DC-DC flyback. However, this device was designed assuming much higher voltages so the under-voltage lock-out will prevent it from working in the range you specified above:
We do have our next-gen PWM controller which has lower standby power which is the UCC28C55. Unfortunately, it is not as low as the UCC28730.
Here are some reference designs based on various parts which may help you get started.
I hope this answers your question.