This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For the LM5155 Application Report "SNVA824 ",I need your help.
1.Why maximum ripple ratio occurs at a duty cycle of 33%?if booster output 12V,is this duty cycle “33%” will changed?
2.A maximum ripple ratio is between 30% and 70% ,The following Equation use the ripple ratio is 60%,How do you decide the value to use,why not 30%?
Hi Bruce,
1. You can find the result by knowing that ripple ratio means ripple current / inductor current. Maximum ripple ratio occurs at a duty cycle of 33% independent of output voltage.
2.As described in this section: A maximum ripple ratio between 30% and 70% results in a good balance between the power loss of the inductor, the down slope of the inductor current and the right-half plane zero frequency. It is a tradeoff for the designer to meet the application requirements.
Best Regards,
Feng Ji