This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92200: Inductor current ripple >300mA requirement

Part Number: TPS92200

Hi TI,

The TPS92200 datasheet stated that the Inductor current ripple >300mA requirement, even smaller inductor value is required in order to meet the high inductor current ripple to assure loop stability.

What if I set the ILED max to 300mA and below by using very low duty cycle? It means the current ripple ratio is >50% and inductor occur discontinuous conduction mode, thus efficiency and power loss should be in bad performance. Please advice. 

Thanks and regards,

ZL Woon