This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8764-Q1: VIO for GPIO4,GPIO7,GPIO8 and GPIO9

Part Number: LP8764-Q1

If we

The GPIOs (GPIO4,GPIO7,GPIO8 and GPIO9)  seem to the in the LDOINT domain (which I think is 1.8V). Is it possible to drive these signals with 3V3 signal when configured as input ? (Especially GPIO4 configured as Enable)

Where in the datasheet does it mention that these GPIOs are in the LDOINT domain ?