Other Parts Discussed in Thread: CSD17318Q2
Hi Team,
I interested to know if we can use BQ24170EVM-610-15V module with minimum or no changes to use it in our proto device for input power of 15V, 230W (around 15A) to charge a 3S2P Battery (12.6V; 4.2V/ each cell).
Please let me know if the eval module can withstand 15A, input current. If Yes, please let me know the possible changes to be done on the eval module for that purpose. If not, please suggest a suitable Evaluation module for above mentioned application, to quickly procure and build our proto device.
Charging Voltage for Battery: 12.69V
Charging Current for Battery: 1.9A
Please let me know if you need any further information.