This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS543C20A: TPS543C20ARVFR can not work correct

Part Number: TPS543C20A


Hi team

My customer used the TPS543C20ARVFR for 12V to  5V & 3.3V, 5V & 3.3V the max output both are 25A (combine max output power 125W ), and OCP each needs 30A.

They found the following issue:

Ch3 is 5V switching
Ch4 is 3V3 switching

1.  Large and small waves appearing in the no-load state

2. When large and small waves appear during loading, the PWM height will drop

to 1A

to 2A

to 3A the switch voltage is about 8V5


3. When a single group loads more than 7A, the 5V and 3V3 output are both out of control


Thanks and regards