This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC12041-Q1: Whether or not a pull-up resistor is required when the SYNC_OK pin is not used.

Part Number: UCC12041-Q1

Hi Team,

The datasheet says to put a 100 kΩ pull-up resistor on the SYNK_OK pin,
but I do not need output confirmation on the SYNK_OK pin.

In such a case, is it safe without a pull-up resistor?

Regards,
Hamashima