Other Parts Discussed in Thread: BQ24780,
We have a design using BQ24780 where we are experiencing a strange condition on power-up. During switch on, VCC becomes higher than VIN (24V), causing the device to go into OVP protection and de-assert ACOK. The device then attempts to switch on, causing the spike again. This repeats at several hundred Hz.
The peak of VCC is observed to be around 28V.
Here is the schematic
The charge current is set to 5A, VIN is 24V and the battery is 3S. When a load of around 0.8A or more is present on VSYS when the charger is switched on, it enters this invalid condition. This happens after the AC deglitch delay, eg 1.3 seonds after the adapter is plugged in. No noise or transients are observalbe at VIN, the only place this is observed is at C11 and both sides of R7, and at VCC.
A diode from VCC to VIN (cathode at VIN) solves the issue, but this allows VBATT to be present at the charger port so is undesirable.
What could be causing VCC to go higher than VIN? It happens during the final stages of switch on of ACFET and RBFET. I can respond with oscilloscope traces of the problem in hand if required.