Other Parts Discussed in Thread: BQSTUDIO,
Hi Experts,
Posting on behalf of my customer who has some problems when using BQStudio.
The picture shows the data monitored by BQ76942(I use the BQStudio):

I connected three batteries, and the voltage of each battery is around 4V.
But the data measured by the chip is far from the actual situation (the voltage of cell1 is 0.2V and the voltage of cell2 is 1.7V).
I don't know if it's my circuit design problem. The picture below shows the circuit I designed.

I wonder if it is the measurement error caused by the circuit design.
If your company can give advice, I will be very grateful.
Regards,
Archie A.