This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV751: About Output voltage setting

Part Number: TLV751

Hi team,

In datasheet, the output voltage fixed option is 0.65V to 5.0V. 

How we can reach the output fixed 0.65V product page?

And if we use the adjustable option set 0.55V output, is it correct that set FBx pin connect to OUTx directly?

Best regards,

teritama

  • Hi Teritama,

    I will look into this and get back to you early next week. Apologies for the delay.

    BR,

    Erin

  • HI Teritama, 

    Apologies for delay. We do not have an orderable part number for fixed 0.65V out. The datasheet showcases the range of the output, but there is currently no demand for TLV751 0.65V output. 

    You can achieve 0.55V out on the adjustable version by connecting the output pin to the feedback pin. 

    If you are looking for 0.55-0.65V output, I recommend TPS7A94

    I hope this is helpful, please let me know if you have additional questions. 

    Erin