Other Parts Discussed in Thread: LM61480
Referencing:
Current PCB uses TPS54561 for +5V and -5V supplies. Load is a LED where Anode = +5V, Cathode = -5V. Iout = 2.8A from each supply
In this configuration an external diode is used to bypass the TPS54561 N-FET (Async DCDC mode?) without this diode the supplies do not start.
Is this due to the over-current limit on the TPS54561 or another feature? I notice the LM61480 specifically mentions Reverse current limit, whereas the TPS54561 datasheet does not appear to.
Regards,
Roy