Dears,
Regarding TPS53622, when modifying the firmware of TPS53622 with an input voltage range of 5V, it was found that VIN-ON and VIN_ UV values are not very friendly, VIN_ ON does not have a 5.0V modification option, but it has 5.25 but is not suitable for working environments with 5V input, and can only be set to 4V.
The first modified one with a VIN_ ON<VIN_ UV