The driver UCC27511AQ was damaged whenever the PFC voltage of 390V builts up (whenever IC comes into action which is above 65V output )
Mainly PIN 1 (VDD) and PIN 2((out1) tracks were damaging. Is there anything to do with the ground connections? ( because GND pin of IC is connected to AGND and 15V IC power supply is connected to PGND and they both are shorted through a 0 ohm resistor)power_control_merged.pdf
I am attaching a PDF of the PFC section and auxiliary supply section for your reference