Hi team,
An inrush current of approximately 3 A was observed from the TPS63060 during startup in a circuit using the TPS63060.
The control current of this device is set at 2.25A, but if it is an instantaneous inrush current at startup, would 3A flow through the upper part of the device?
The steady-state operating current is about 400~500mA.
Sincerely.
Ryu