Other Parts Discussed in Thread: TUSB1210, TPS25750
Hello,
I plan to design a type c interface with TPS25820 and TUSB1210. The requirement is
1. support up to 3.0 version.
2. support host and devcie mode as well as USB 2.0 OTG devices.
the architecture I plan to impelement is simply shown as below
A few question may ask for answer.
1. do I need to wire the /sink signal to the MPU to detect whehter the port should be activated as host (eg. a usb stick is inserted) or device (eg. a laptop is connected)
2. According to USB-IF document, OTG is not compatible with type c. Is it possible to use an adapter which connect the CC1,CC2 to the ID pin?
3. if #2 can work, how should I handle the ID pin of TUSB1210?
thanks in advance.