I am evaluating TLV61220.
R1 = 1MΩ, R2 = 110kΩ, L1 = 4.7uH, C2 = 10uF.
The output load is almost no load.
Then if Vin = 4.94V, then VFB = 720mV and VOUT = 4.40V.
From the resistance values of R1 and R2, I would like the output voltage to be approximately 5.0V.
Please give me a hint that the output voltage will be the intended value.
thank you.
I don't care if it's a guess, so I'd appreciate it if you could give me some hints.