Hey Support.
If the resistor R9 (on the back of the board) is fitted with a resistor of 11.5k on the TPSM63610EVM module, is the output voltage then 12V? Thanks for info.
Regards Norbert
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Support.
If the resistor R9 (on the back of the board) is fitted with a resistor of 11.5k on the TPSM63610EVM module, is the output voltage then 12V? Thanks for info.
Regards Norbert
Hello Norbert,
The subject matter expert is currently out of office, we will provide an update by end of the day tomorrow 5/31.
Regards,
Oscar Ambriz
Hi Norbert,
Yes. That is correct. Just keep in mind that this is a buck converter so input is higher than output.
Regards,
Richard