Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO
Dear Sirs and Madams,
We are considering BQ27520-G4.
The specifications of the batteries used in operation verification are 3.7V, 1500mAh, and 5.7Wh.
Successfully got the ID from GPCCHEM of TI website and am using ChemID : 0321.
Initially, we used CHEM ID : 1200, which is the best reported by GCPCHEM, but RUP_DIS becomes 'H' during the learning cycle test, so we use CHEM ID :0321.
By adopting CHEM ID 0321, RUP_DIS can maintain 'L'.
I think VOK is also trending normally.
However, even after finishing the learning cycle, the Update Status in the data memory remains 0x00 and does not become 0x02.
I have investigated E2E, TRM and "Achieving The Successful Learning Cycle" variously, but I have not been able to identify whether it is a problem.
The settings for each current are as follows :
- Taper current : 150mA (=C/10)
- Dsg current threshold : 90mA
- Chg current threshold : 110mA
- Quit current : 75mA (=C/20)
It meets the following conditions:
- “Dsg current > Quit current”
- “Taper current > Chg current > Quit current”
Do you know what is the reason why Update Status remains 0x00 and does not change to 0x02?
Only "Cycle Count" and "Cell 0 V at Chg term" of Gas Gauging and "CC Offset" of Calibration are updated.
/* Achieving The Successful Learning Cycle document URL */
Regards,
MM