This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS66020: Is there a way to make it so the output of the PD controller connected to the TPS66020 is regulated at 65W while the input can be anything from 11V to 32V.

Part Number: TPS66020
Other Parts Discussed in Thread: TPS65987D, BQ25731, TPS25750, TPS25750EVM

I am trying to connect the TPS65987D to a TPS66020, but I need the output when the circuit is a Source to be at a regulated 65W. The USB Type C port can can take in freely anything from 11V to 32V when the circuit is acting as the Sink. I need to know if I need to connect a Buck-Boost to my output or if a should not worry about using the TPS66020.

Thank you