Hello expert,
For the datasheet I have some question below:
1.VOUT adjustable from 1 V to 95% of VIN——what is the input voltage and output power for this case?I test my board with Vo=7V and find the Vin min is 7.9V to ensure this output,it is just 89.5%.A big gap from 95%.
2.0.4-V dropout with 4-A load (typical)——Is this conflict with the statement 1?
3.High side MOSFET RDS(ON) 41 82 mΩ——Is this conflict with the statement 1? When output 6A,even the duty is 100%,the HS mos will create a voltage drop of 0.49V. ——Is this conflict with the statement 1 too?
So,how to define the minimum input voltage when Vo=7V,consider the worse case?