Hi Team,
my customer is searching for load switch device with OVP/OCP used in smartphone.
Vin= 3-5.5V, Vin max = 28V, Iout=2A, Ron max = 120mohm, reverse block.
ESD: IEC61000-4-2, air discharge >=12KV, contact discharge >= 6kV? Or is there part can meet this? Thanks.
similar function you can refer to FPF2495C. in eFuse: p2p with FPF2495 - Power management forum - Power management - TI E2E support forums, there is TPS25948, but there seems no IEC61000-4-2. Is there other suitable device? Thanks.
BRs
Given