Other Parts Discussed in Thread: LM7800, LM5060-Q1, LM74910-Q1
Hi
Could you help check the below LM74800 schematic and any need to adjust
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you help check the below LM74800 schematic and any need to adjust
Thanks
Hi Gareth,
Please see my review comments below,
1. Leave the thermal PAD / RTN pin floating. Connecting it to GND will disable reverse polalrity protection.
2. For Input TVS use SMBJ33CA to pass Automotive tests such as ISO7637-2 and ISO16750-2. For more understanding on TVS selection, please refer to section. '11.2 TVS Selection for 12-V Battery Systems' of datasheet.
Remaining schematic looks good to me.
Hi Praveen GD
Hi Praveen GD
Could you help check the below LM74800 layout PDF
PCB layers: 10L
The location of the IC and surrounding parts is in the area indicated by the frame line of my map. Thanks.


Hi Gareth,
It is difficult to review the layout if it is shared as pdf and also without silkscreen. We can review the layout if you can share the CAD source files in Altium or Allegro. If not possible, customer can self-review the schematics using the layout guidelines below.