Hello Experts
I am using Synchronous rectification at the PSFB secondary side where the load current flow is from source to drain. So my doubt is whether this ucc21732 can be used for getting of desat protection ?
Thanks and regards
Anoop kumar N
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Experts
I am using Synchronous rectification at the PSFB secondary side where the load current flow is from source to drain. So my doubt is whether this ucc21732 can be used for getting of desat protection ?
Thanks and regards
Anoop kumar N
Hi Anoop,
The short circuit protection of the gate driver is essentially a comparator which is referenced to the SOURCE of the MOSFET.
The customer could use the UCC21732 OC-pin comparator input to measure the voltage drop across a shunt resistor that would need to be placed in the main power loop. Since this shunt resistor would be in the gate loop path the voltage will also affect the gate voltage. The shunt resistor would add additional power dissipation, which could be okay depending on the load current level.
Best regards,
Andy Robles
hi andy, thank you for the reply.
schematic was ready where i connected the drain point to the oc pin. later i realized that normal load current flow is from source to drain. adding this this resistr in power loop not at all a feasible solution. because load current is around 100amps
Thanks and regards
Anoop kumar N
Hi Anoop,
For the OC-pin in UCC21732 to be used in DESAT it needs to have the configuration shown in Figure 54 of the UCC21732 datasheet:
Having the current flow from Source to Drain would apply a negative voltage on the Drain net with respect to the Source.This means that the traditional circuit implementation would not work in your application.
I believe this circuit could potentially work if you were to design an inverting buffer circuit between the Drain and the Cathode of the high voltage DESAT diode, but I have never seen this type of circuit implemented myself before.
Best regards,
Andy Robles